Banner

Get rid of cables with Genesis Zircon 500 Wireless - a wireless model with a symmetrical body, which allows you to use up to 3 connectivity modes. Bet on the proven Pixart PMW3325 optical sensor and increase your precision in game. Want to react faster? No worries. Mechanical Kailh 4.0 switches with a life span of 60 million clicks mean better dynamics and a well felt trigger point, which fans of the RTS and FPS genres will appreciate. Don't believe it? Take the challenge and see for yourself. With Genesis Zircon 500 Wirelessyour gameplay can look completely different.

Banner

CONNECTIVITY? MATCH IT TO YOUR OWN STYLE

Efficient 2.4 GHz radio connection with low latency, energy-efficient communication thanks to BT 5.0 or classic cable mode. Decide for yourself and match the Genesis Zircon 500 Wireless to your own playing style. Use the full potential of the built-in 300 mAh battery and play without interruption. And if you're surprised by low power, just plug the Genesis Zircon 500 Wireless into your computer, using the included cable with a USB-C plug. You don't have to put the mouse down. You can keep playing the game while charging your mouse at the same time. It's simple.

GREATER PRECISION = GREATER CHANCE OF WINNING

Skills are important, but equally important is a proven sensor that will allow you to get the most out of them. We've equipped the Genesis Zircon 500 Wireless with the acclaimed Pixart PMW3325 optical sensor with a maximum resolution of 10,000 DPI, which will faithfully reproduce your every move even at offsets of 100 inches per second. Expect confident handling and lightning-fast gliding? Sliders made of Teflon will help you do just that. Smooth movement on multiple surfaces - that's what the Genesis Zircon 500 Wireless is all about.

EVEN BETTER DYNAMICS

Meet the latest Kailh 4.0 mechanical switches. Be amazed by their high durability (60 million clicks), bounce dynamics and clarity. Gain an edge with lightning-fast button return and quick and clear activation. Mechanical switches will provide better auto-fire control in FPS games and faster response in dynamic RTS titles. And that's not all. You can program the Genesis Zircon 500 Wirelessbuttons however you want. Assign actions and macros to them. Be one step ahead of your rivals.

79 GRAMS OF COMFORT

Full symmetry and 79 grams of weight. We designed the Genesis Zircon 500 Wireless to meet the expectations of even the most demanding gamers. Subtly contoured sides and a clearly defined back mean full control and a more secure grip even during high-speed skirmishes, while buttons separated from the top mean even better resilience. Whether you use a palm or fingertip grip, with the Genesis Zircon 500 Wirelessyou will forget about hand pain.

DEDICATED SOFTWARE

Use the dedicated software and create a unique configuration. Change the resolution of the sensor, the actions assigned to the keys and set your own macros to support you in gameplay. Operation of the control application is simple. Both less and more advanced users will easily find their way around it.