White gaming mouse with multiple buttons and a sleek, ergonomic design.

 

Get rid of cables with Genesis Zircon 500 G2 - a wireless model with a symmetrical, slightly enlarged body, which will allow you to use up to 3 connectivity modes. Bet on the proven Pixart PMW3325 optical sensor and increase your precision in gameplay. Want to react faster? No worries. Huano 90M Purple mechanical switches with a life span of 90 million clicks mean better dynamics and a well felt trigger point, which fans of the RTS and FPS genres will appreciate. Don't believe it? Take the challenge and see for yourself. With Genesis Zircon 500 G2 woja gameplay can look completely different.

Graphic highlighting features of a gaming product with icons and descriptive text.
A white keyboard with colorful backlighting and a matching white gaming mouse on a desk mat.

LINK? MATCH IT TO YOUR OWN STYLE

Efficient 2.4GHz radio connection with low latency, energy-efficient communication thanks to BT 5.0 or classic cable mode. Decide for yourself and match the Genesis Zircon 500 Wireless to your own gaming style. Use the full potential of the built-in 300 mAh battery and play without interruption. And if you're surprised by low power, just plug the Genesis Zircon 500 G2 into your computer, using the included cable with a USB-C plug. You don't have to put the mouse down. You can keep playing the game while charging your mouse at the same time. It's simple.

 

Wireless mouse with a scrolling wheel and a detachable connection device.

GREATER PRECISION = GREATER CHANCE OF WINNING

Skills are important, but equally important is a proven sensor that will allow you to get the most out of them. We've equipped the Genesis Zircon 500 G2 with the acclaimed Pixart PMW3325 optical sensor with a maximum resolution of 10,000 DPI, which will faithfully reproduce your every move even at offsets of 100 inches per second. Expect confident handling and lightning-fast gliding? Sliders made of Teflon will help you do just that. Smooth movement on multiple surfaces - that's what the Genesis Zircon 500 G2 is all about.

 

White gaming mouse with a connection port and a glowing light on the bottom.

EVEN BETTER DYNAMICS

Meet the top Huano 90M Purple mechanical switches. Be amazed by their extraordinary durability (90 million clicks), rebound dynamics and the clarity of each press. Thanks to the reduced pressure force (by as much as 5 grams!), the activation of each click has become ultra-fast, and you gain an advantage with lightning-fast return to the point of activation of the buttons. What does this mean in practice? Mechanical switches will provide better auto-fire control in FPS games and faster response in dynamic RTS titles. And that's not all. You can program the additional buttons on the Genesis Zircon 500 G2 however you want. Assign actions and macros to them. Always be one step ahead of your rivals.

 

A white computer mouse with a visible wheel and a compartment for a connection device.

NOW ONLY 52 GRAMS OF COMFORT

Full symmetry, a slightly enlarged body, yet only 52 grams in weight. We designed the Genesis Zircon 500 G2 according to the suggestions of gamers to meet the expectations of even the most demanding users. The subtly contoured sides and clearly outlined back mean full control and a more secure grip even during high-speed skirmishes, while the buttons separated from the top mean even better resilience. Not enough? The Zircon G2 also features top-notch plastic and a perfect fit of the components. Whether you use a palm, claw or fingertip grip, the Genesis Zircon 500 G2 will fit you and your style.

 

White mouse shown in motion above a red and black background.

DEDICATED SOFTWARE

Use the dedicated software and create a unique configuration tailored to you. Change the resolution of the sensor, the actions assigned to the buttons and set custom macros that will support you in the gameplay allowing you to gain precious fractions of seconds that decide the win. Operation of the control application is simple. Both less and more advanced users will easily find their way around it, so that the Zircon 500 G2 mouse is for one thing - winning!

 

Three software interface windows showing settings for a customizable gaming mouse.
A white mouse and a black mouse side by side on a dark background with buttons shown.