Meet one of the most advanced mice on the market. Here is the GENESIS Zircon XIII - a complete design offering everything you really need. Full hardware customization (interchangeable switches, distances, springs), one of the best sensors in the world (Pixart PAW3395) and wireless connectivity technology (RapidSpeed™ Wireless) for truly wired performance, and that's not all. With GENESIS Zircon XIII, the game is just beginning.


The unity of the hand with the mouse is a key aspect in any game, because it is thanks to it that you win or lose. This is the reason why some models - despite great parameters - do not perform well in practice. When designing our latest mouse, we knew that we could solve this problem with one thing - full personalization. Only it could meet the expectations of both the one who is looking for an uncomplicated, comfortable lump expecting stability while driving, and the professional who wants to adjust the crispness of the switch and the stroke of the main button with an accuracy of 0.1 mm. Thus was born GENESIS Zircon XIII - a mouse that will change the face of your gameplay, the culmination of 13 years of experience of the GENESIS brand.

Welcome one of the world's most modern and advanced optical sensors. The Pixart PAW3395 not only offers excellent cursor feel and responsiveness. It's also a guarantee of flawless tracking even at a maximum speed of 16.51 m/s and 50G acceleration. This gives you the confidence that everything that happens on the screen will depend only on your skills.
Get a head start with Motion Sync, an all-new, refined technology that improves reporting (pooling rate). It ensures that sending mouse position data to the computer is fully synchronized with receiving it. This, in turn, ensures not only smoother movement, but also greater efficiency in registering every move, even the slightest one, or action. Don't let yourself be dominated and bet on a solution that guarantees real benefits.

Decide for yourself how you want your copy of the GENESIS Zircon XIII to work. Thanks to the customisation options, you can easily adjust the force needed to activate the button (dedicated springs), their stroke (special spacers), or replace the microswitches of the main buttons (you will find up to 2 additional types in the set, including the Huano Silent switches). All this without technical skills or soldering, using just one included tool.

Full comfort is due to both the configuration and the well-thought-out body, which is perfect for the hand of right-handed gamers. What's more, you can easily adjust the back of the mouse to suit your needs thanks to the interchangeable panels. As well as stability - just use the included anti-slip grips and stick them on the parts of the mouse you want. It's as simple as that.

GENESIS Zircon XIII is quality that will surprise you. In addition to the Pixart PAW3395 sensor, you'll find the highest quality components inside, because only they can ensure trouble-free gaming for a long time. Enjoy the replaceable main button switches (Kailh 8.0 with 80 million clicks) and the robust TTC Gold encoder. You don't have to worry about the sliders either. They are made of PTFE and their rounded edges have a positive effect on the smoothness of movement. You'll also find an extra set of them in the box. All this is to ensure that your mouse serves you for as long as possible.

Wired performance, wireless convenience. Meet RapidSpeed™ Wireless - the connectivity technology designed for the most demanding gamers. Lightning-fast data transfer, zero interference and wired precision - and that's not all. You'll also enjoy up to 100 hours of non-stop play thanks to the 600 mAh battery. And if you want to use the mouse in the traditional way, you can do so using the lightweight and robust Paracord USB-C cable.

We haven't forgotten about the additional features that will make using the GENESIS Zircon XIII quick and easy. The slider located at the bottom will allow you to switch between wired mode, wireless mode and turn off the backlight. A dedicated button, on the other hand, will allow you to change the backlight mode. Combined with the built-in memory and advanced software, this gives you almost unlimited possibilities and freedom of use.