Banner

Say hello to one of the lightest wired mice on the market. Behold the GENESIS Krypton 660 - a design weighing just 49 grams that will allow you to react even faster. You'll also be helped by a flexible Paracord cable and a PAW3327 optical sensor capable of tracking movements as fast as 220 inches per second. As if that wasn't enough, the GENESIS Krypton 660 is also about comfort and functionality through dedicated software. Get to know it closer and see what else it will surprise you with.

 

Banner

BET ON PRECISION

A low-quality sensor is an element that can ruin gameplay at the least opportune moment. With GENESIS Krypton 660, you can forget about any anomalies that can disrupt it. PAW3327 is the absence of positive and negative acceleration phenomena and loss of tracking even with movements of 220 inches/second and accelerations of 30 G. Accurate tracking - millimeter by millimeter - means you can be sure that defeating your opponent will depend only on your own skills.

A WEIGHT OF ONLY 49 GRAMS

Are you a low sense gamer and often lift your mouse? Or do you simply appreciate designs that allow you to react faster and don't get tired after a long session? No matter which group you belong to, the GENESIS Krypton 660 will meet your expectations. Its weight (49 grams) was achieved by our thoughtful choice of materials, the use of a lightweight Paracord cable and the unique cutouts present on the bottom. All this makes the GENESIS Krypton 660 we can proudly call one of the lightest mice on the market.

EVEN MORE CONVENIENTLY

The body of the GENESIS Krypton 660 was designed with gamers using palm and claw grips in mind. This means special profiling to ensure stable hand positioning and raise comfort to the maximum during long hours of gaming. Zero hand and wrist pain, confident handling and even easier mouse lift. GENESIS Krypton 660 is a real advantage in any situation.

BECAUSE IT'S THE INSIDE THAT MATTERS

High quality workmanship - this is the result of using good quality materials, but also the best quality components. Among them you will find Huano Purple mechanical microswitches distinguished by a perceptible and very dynamic click, endurance of up to 90 million clicks and moderate pressure force (60 g), as well as a durable and appreciated by many TTC White encoder with a perceptible scroll stroke. High-quality PTFE sliders are also not insignificant. Smooth movement on multiple surfaces? Not a problem from now on.

FULL CONTROL

Create profiles, record macro combinations, personalize buttons and backlighting, all with the dedicated GENESIS app. No worries - it's easy to read and easy to use. With it, you will unleash the maximum potential of the GENESIS Krypton 660 and increase your effectiveness. See how easy it is.