The Delizia pizza oven by G3 Ferrari quickly reaches the ideal 400° for baking in just a few minutes: you’ll see that 5 will be more than enough.
The oven features two heating elements, positioned respectively in the dome and beneath the cooking chamber floor, with low power consumption: max 1200Wh

Choose quality without compromising on style. The Delizia pizza oven is the only one to offer the widest range of colors available on the market.
There’s sure to be one that’s perfect for you, too.

The long history of the Delizia pizza oven and over 50 years of the G3 Ferrari brand have led to improvements in every detail, including the recipe book, which features well over 100 different recipes: try it for yourself.

Pizza is one of the iconic dishes of the Italian culinary tradition. Although it is difficult to pinpoint its exact origins, many believe it dates back to between the 16th and 17th centuries, in what was then the Kingdom of Naples. It was certainly Raffaele Esposito who first brought it prestige and fame when, in 1889, he dedicated a pizza to Queen Margherita of Savoy, from whom it took its name. With the original Delizia oven, you can bake excellent, fragrant pizzas at home too, thanks to the research and innovation that have defined the G3 Ferrari brand for decades.

The food-grade aluminum peels ensure greater hygiene over time.
The plastic handle provides proper insulation and a secure grip.

Thanks to their larger size, with a diameter of 28 cm, even large pizzas can be easily prepared and placed on the oven deck.

Special 31 cm refractory stone weighing 1.36 kg, made from natural materials suitable for food cooking. It ensures the right moisture exchange.
With use, the stone is intended to darken, just like the ovens in traditional pizzerias.

The special circular design of the upper heating element ensures exceptional results and more even cooking of the crust.