Banner

Do you love long gaming sessions, but during them you always suffer from back or cervical pain? Often this is due to the lack of adjustment and profiling of the seat, which has nothing to do with the correct posture in front of the computer. Keeping in mind the comfort, health and expectations of gamers around the world, we have improved the Genesis Astat 700 to meet the expectations of even the most demanding users. Even stronger material and better adjustment of moving parts. This is the Genesis Astat 700 G2.

INNOVATIVE 8-RIB DESIGN

Proper profiling of the chair is the most important aspect that directly affects your health. Just as your spine is a support for your whole body, the Astat 700 G2 chair provides external support, relieving your back in each section of the spine. This is possible thanks to the 8-rib ExoBase™ design, which is a faithful reflection of how your spine should be arranged in the lumbar part. This element can be adjusted in up to 3 positions. Thanks to this, you will avoid back pain in the most vulnerable sections. You can be sure that the lack of pain will positively affect your concentration, which is highly likely to translate to better results achieved in the game.

SEAT DEPTH CEASES TO BE A PROBLEM

Speaking of full adjustment, we have not forgotten about the seat. Few seats can boast depth adjustment. This function is useful for both short and tall people because it directly affects the comfort of the backrest and muscle relaxation.

ADJUST THE BACKREST ANGLE

Want to relax after a long game? With the Astat 700 G2 you can do it in just a few seconds. Change the angle of inclination of the backrest and it will lock it in the position of your choice. It's that simple.

TAKE CARE OF YOUR NECK

Did you know that many spinal injuries are related to the cervical spine? Most of the pain is caused by prolonged, excessive bending and incorrect inclination. The headrest of the Astat 700 G2 chair will allow you to set the angle of inclination and height so that you will forever get rid of the radiant pain that could hinder you.

EXCELLENT SUPPORT FOR YOUR ARMS AND HANDS

We have not forgotten about 3D armrests. You can easily adjust their height, extension and even the direction of position. Forget about them moving on their own. We've stiffened the armrests so that full control over their position depends only on you. Their soft finish gives great comfort.

ADJUST WHATEVER YOU WANT

The pain accompanying the players results primarily from the universal nature of chairs. We know perfectly well that each one of us is different, and the key to success is an armchair with elements that can be adapted to the individual needs of the player. This is how Astat 700 G2 was created, which thanks to adjustable elements will adapt to your position in front of the computer, but above all - your own posture. Tilt, lower and create your own individual, unique setting. Make the gameplay a real relaxation.

FEEL THE COMFORT REGARDLESS OF THE TEMPERATURE

Tired of leather finishes and are looking for an armchair that will give you with full ventilation? The backrest and headrest of the chair are made of mesh, breathable PureFlowPLUS™ material. It is not only easy to clean, but so durable and resilient that the whole seat has also been made from it. There is no foam which over time can crumple and affect your posture. Forget about the chair getting too hot and focus on what really matters.

EVEN MORE DURABLE

If you are looking for an armchair that will last you many years, the Genesis Astat 700 G2 is perfect for this role. In order to meet the expectations of demanding users, we reinforced the key components of the design to make it even more durable and provide greater comfort during long hours sessions. The well-known 5-armed aluminum base with a unique design could not be missed either.

CAREGLIDE™ WHEELS

If you want to move it around the place, you can do it easily with 60mm CareGlide™ wheels covered with a special layer that prevents scratching of the ground and ensures smooth movement on any surface.

DESIGN THAT EVERY GAMER WILL LOVE

Do you want to match the Genesis Astat 700 G2 to your space? Its distinctive gaming design will make it easy to fit wherever you want. What's more, the Genesis Astat 700 G2 is available in two color options. Choose your favorite one and create a place with a unique atmosphere.

MEET THE DIMENSIONS OF THE GENESIS ASTAT 700 G2